The ideal
combination

Minimum cost and maximum performance
View report

Sandbox Achieve the optimum axle-guide linkage profile

Introducing HALL® Hydraulic Elastomers

Good curving behaviour and stable high-speed running in axle guide bearings have traditionally been seen as mutually exclusive characteristics – if you achieve one, you compromise on the other. Now, however, there’s no longer any need to compromise, thanks to HALL® hydraulic axle guide bearings.

The ideal combination of minimum cost and maximum performance

  • Frequency-dependent performance delivers low stiffness in curves and greater stiffness at high speeds
  • Reduced friction conserves energy and cuts your lifecycle costs
  • Easy fitting and exchange ability with conventional bearings keep your track access charges to an absolute minimum
  • Immediate usability – there’s no need to modify your vehicles
  • Reduction of wear on wheels and rails
  • Greater protection of vehicles and platforms
Button Text

Calculate your cost savings with HALL®

Try our online calculator to identify how much you could save each year by adding HALL® to your vehicles.

See your savings now
Achieve the perfect profile

HALL® – Hydraulic axle guide bearings

With HALL®, you can combine the low longitudinal stiffness for curves with the high longitudinal stiffness for movement in a straight line in a single component. The hydraulics integrated hydraulics lead to frequency dependent changes of the longitudinal stiffness.

The hydraulic axle guide bearing can be designed in such a way that a low stiffness is automatically available during steady adjusting movements when entering or exiting a curve. The bearing stiffness increases during dynamic excitation at higher speeds. As the HALL® fits in the existing space for conventional axle guide bearing, it can be integrated in new, as well as existing, vehicles without structural modifications to the bogie.

tunnel with lights traveling fast

What could you save with HALL®?

Try our online calculator to discover how much you could save by adding HALL® to your rail vehicles. Once you’ve tried the online version, get in touch with us for an even more detailed picture of your savings, taking into account:

  • The number of years between changing parts
  • Class of train
  • Fuel type
  • Wear on bearings
  • Reprofiling wheels

These initial results are based on simulations using a fixed and varied route (varied meaning some turns and some straights), using an approved 185hb/m train.

To calculate your savings, simply select the appropriate information below.

This calculation is just the beginning

For a more detailed breakdown of the total savings you could achieve, request a meeting with a member of the Trelleborg team.

Contact us

Engineered to perform

Diagram of anti vibration tool
Longitudinal Stiffness Dynamic / Quasi-static  » 4-10
Graph
Switching Frequency 0.4-2 Hz
(project specific)
Lateral stiffness 4-30 kN/mm
(project specific)
Comes in a variety of dimensions so can simply replace existing bushes
Quasi static longitudinal stiffness 2-7 kN/mm
(project specific)

Reducing wear, cutting costs

Infrastructure maintenance costs represent a significant part of the overall cost of railway operations. Increasing axle loads, higher speeds and the greater axle control stiffness required have seen this cost spiral further in recent years.

Recent intensive studies in the UK and Sweden on the relationship between vehicle properties and the wear of wheel and rail were conducted, leading to new fee models for the track access. These models reward flexible axle control with lower fees.

Measurements in the vehicles secured with HALL® show a significant regression of wear and rolling contact fatigue (RCF) in wheels and rails.

Train platform
Train traveling at speed

1.1 million miles without losing performance

In a recent customer test, HALL® hydraulic axle guide bearings were shown to continue delivering the optimum combination of outstanding curving behavior and stable high-speed running, even after 1.1 million miles.

Train
Train tracks
Overhead lines
Train
Train tracks
Overhead lines

What’s a Rich Text element?

The rich text element allows you to create and format headings, paragraphs, blockquotes, images, and video all in one place instead of having to add and format them individually. Just double-click and easily create content.

  1. afsdgpkdsafg;lsdfkj;glksfd
  2. sdfg;lksfd;glkjsdfg
  3. sd;fkgjsdf;lkgjsdf;lkg

Static and dynamic content editing

A rich text element can be used with static or dynamic content. For static content, just drop it into any page and begin editing. For dynamic content, add a rich text field to any collection and then connect a rich text element to that field in the settings panel. Voila!

How to customize formatting for each rich text

Headings, paragraphs, blockquotes, figures, images, and figure captions can all be styled after a class is added to the rich text element using the "When inside of" nested selector system.

A more comfortable ride for your customers and business

Introducing Tilt Cab Mount

Offer your skid-steer and compact-track loader customers a new standard of comfort and quality. Thanks to one easy-to-fit Tilt Cab Mount, you can keep noise and vibration to a minimum, drastically reduce wear and tear, and give operators a far more comfortable ride.

One universal solution for lasting tilt cab comfort

  • Easy cab installation thanks to a tapered metal cup that guides the cab into the frame bracket removing the need for shims
  • Increases lifetime vehicle performance and reduces downtime
  • Engineered with the highest quality components
  • Designed to support cab alignment during tilting for easy maintenance
  • Improved axial stability for a more comfortable ride

Request a call

To learn more about how Tilt Cab Mount can benefit you and your customers, register your interest today and a Trelleborg representative will be in touch.

Request  callback
Request a call

Want to discuss HALL® with a Trelleborg specialist?

For a closer investigation of the properties of HALL®, and to understand the precise cost benefits it could give you, fill in this short form and a member of the Trelleborg team will be in touch to arrange a call at a convenient time.

*Required field

Thank you!
Your submission has been received!
Oops! Something went wrong while submitting the form.
close