The ideal
combination

Minimum cost and maximum performance
View report

Achieve the optimum axle-guide linkage profile

Introducing HALL® Hydraulic Elastomers

Good curving behaviour and stable high-speed running in axle guide bearings have traditionally been seen as mutually exclusive characteristics – if you achieve one, you compromise on the other. Now, however, there’s no longer any need to compromise, thanks to HALL® hydraulic axle guide bearings.

The ideal combination of minimum cost and maximum performance

  • Frequency-dependent performance delivers low stiffness in curves and greater stiffness at high speeds
  • Reduced friction conserves energy and cuts your lifecycle costs
  • Easy fitting and exchange ability with conventional bearings keep your track access charges to an absolute minimum
  • Immediate usability – there’s no need to modify your vehicles
  • Reduction of wear on wheels and rails
  • Greater protection of vehicles and platforms

Calculate your cost savings with HALL®

Try our online calculator to identify how much you could save each year by adding HALL® to your vehicles.

See your savings now
Achieve the perfect profile

HALL® – Hydraulic axle guide bearings

Nordic Railways can benefit from HALL® technology, which offers a unique solution to combine low longitudinal stiffness for curves with high longitudinal stiffness for straight line movement in a single component. HALL® utilizes integrated hydraulics that enable frequency dependent changes in the longitudinal stiffness, with a hydraulic axle guide bearing that automatically provides low stiffness during steady adjusting movements when entering or exiting a curve.

Furthermore, the bearing stiffness increases during dynamic excitation at higher speeds. The best part is that HALL® can be easily integrated into both new and existing vehicles without any structural modifications to the bogie, as it fits into the existing space for conventional axle guide bearings.

What could you save with HALL®?

Try our online calculator to discover how much you could save by adding HALL® to your rail vehicles. Once you’ve tried the online version, get in touch with us for an even more detailed picture of your savings, taking into account:

  • The number of years between changing parts
  • Class of train
  • Fuel type
  • Wear on bearings
  • Reprofiling wheels

These initial results are based on simulations using a fixed and varied route (varied meaning some turns and some straights), using an approved 185hb/m train.

To calculate your savings, simply select the appropriate information below.

This calculation is just the beginning

For a more detailed breakdown of the total savings you could achieve, request a meeting with a member of the Trelleborg team.

Contact us

Engineered to perform

Diagram of anti vibration tool
Longitudinal Stiffness Dynamic / Quasi-static  » 4-10
Graph
Switching Frequency 0.4-2 Hz
(project specific)
Lateral stiffness 4-30 kN/mm
(project specific)
Comes in a variety of dimensions so can simply replace existing bushes
Quasi static longitudinal stiffness 2-7 kN/mm
(project specific)

Reducing wear, cutting costs

Infrastructure maintenance costs represent a significant part of the overall cost of railway operations. Increasing axle loads, higher speeds and the greater axle control stiffness required have seen this cost spiral further in recent years.

Recent intensive studies in the UK and Sweden on the relationship between vehicle properties and the wear of wheel and rail were conducted, leading to new fee models for the track access. These models reward flexible axle control with lower fees.

Measurements in the vehicles secured with HALL® show a significant regression of wear and rolling contact fatigue (RCF) in wheels and rails.

Train tracks
Train traveling at speed

1.1 million miles without losing performance

In a recent customer test, HALL® hydraulic axle guide bearings were shown to continue delivering the optimum combination of outstanding curving behavior and stable high-speed running, even after 1.1 million miles.

Train
Train tracks
Overhead lines
Train
Train tracks
Overhead lines
Request a call

Want to discuss HALL® with a Trelleborg specialist?

For a closer investigation of the properties of HALL®, and to understand the precise cost benefits it could give you, fill in this short form and a member of the Trelleborg team will be in touch to arrange a call at a convenient time.

*Required field

Thank you!
Your submission has been received!
Oops! Something went wrong while submitting the form.
close